Part Number: AM2634-Q1
Tool/software:
Hi
We are using the AM2634-Q1 for our application, and based on our current requirements, the 2MB of internal RAM may not be sufficient. We are planning to add external RAM via the GPMC interface and would appreciate your guidance on the following:
-
Maximum Supported Size:
What is the maximum size of external RAM that can be connected to the AM2634-Q1 via GPMC? Are there any recommended part numbers or memory types (e.g., SRAM/PSRAM) that are known to work well with this device? -
Memory Configuration and Usage:
Once external RAM is connected, how do we configure the application to utilize it? Will the internal OCRAM and external RAM work together as a contiguous memory region, or will they function as separate memory banks?
If there are any reference examples, application notes, or documentation on how to configure and use external RAM with GPMC on AM263x, please share those.
Thanks in advance for your support!