Other Parts Discussed in Thread: MSPM0G3507,
Tool/software:
Team,
Posting on behalf of my customer. They would like to confirm the following works to correctly enable the BSL.
We would like to use BSL option of MSPM0G3507/ MSPM0G3519.
It looks like PA18 default (BSL pin) is high? Therefore, if we put in BSL mode, then we will need to pull it down, correct?
Below is circuit, could you please suggest my understanding is correct? Or need any modification in Boot circuit. 47.5kOhm 1% pull down to GND being implemented if you can't see the image properly.

Thanks,
Tom