Part Number: MSPM0L1105
Tool/software:
MSPM0L1105, I have some questions about the hysteresis of GPIO in this MCU, as follows:
The VDD of the IC is 3.228V
1. There is only one minimum value for hysteresis in the spec, calculated as 0.1x3.228V=0.3228V; What is the maximum value?

2. The IC itself has VIH and VIL, and my understanding of hysteresis can be calculated
Vih(min)=3.228V x 0.7=2.26V.
Vil(max)=3.228V x 0.3=0.968V
So hysteresis=1.292V (2.26V-0.968V)
So what is the meaning of hysteresis in the spec?