This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1104: How to flash code to MSPM0C1104?

Part Number: MSPM0C1104

Tool/software:

I understood now, that the C series does not have the default ROM based BSL, but I don't quite understand how I can flash code to the microcontroller then? Surely SWD will work once, but once a program is flashed to the device, how can I enter the bootloader (using a strapping pin, in case the code is corrupt or doesn't load properly and locks me out that way), and is there an option to flash code using I2C or alternatively UART, similar to the default ROM BSL on other MSPM0 devices?