Part Number: AM2632
Tool/software:
I'm running FreeRTOS, using SDK 10.01.00.31. I have quite a few peripherals configured including the ADC and 3 uarts. But not much code using them for this test. I mention the ADC's because there was an issue in previous SDK's with enabling the ADC's and getting the systick to start correctly. At some point during execution, nothing much happening other than serial comms to a logging port and comms to a TI BQ79361. The BQ runs it's serial at 1Mbit, so there are some 'fast' interrupts from there. I mention the serial ports, because I can make the systick interrupt stop quicker with more serial comms happening.
After running, usually within a minute or 2, the systick interrupt just stops (interrupt 84). When I say stops, the HwiP_irq_handler_c() function is never called again for the systick interrupt. If the ADC is configured to run continually, the HwiP_irq_handler_c() is called for ADC interrupts.
Below is the snapshot of the RTI0 registers when it is in this state. From what I can tell, the timer is still running: RTIFRC0, RTIUC0, and RTICOMP0 are all still being updated. The other register settings appear as expected to me to generate an interrupt, yet none occur. Is there a mask bit somewhere else I can look for to see if it is being masked somewhere else?
If there is a mask bit or some other setting in the RTI0 registers that is incorrect, what might cause that? Again , there are a lot of serial interrupts happening- is there an issue there?
Thanks for you help.
RTI0_RTI0 MSS_GPIO
RTI0_RTIGCTRL 0x00000001 Memory Mapped
RTI0_RTITBCTRL 0x00000000 Memory Mapped
RTI0_RTICAPCTRL 0x00000000 Memory Mapped
RTI0_RTICOMPCTRL 0x00000000 Memory Mapped
RTI0_RTIFRC0 0x000589EB Memory Mapped
RTI0_RTIUC0 0x00004239 Memory Mapped
RTI0_RTICPUC0 0x000061A7 Memory Mapped
RTI0_RTICAFRC0 0x00000000 Memory Mapped
RTI0_RTICAUC0 0x00000000 Memory Mapped
RTI0_RTIFRC1 0x0000875D Memory Mapped
RTI0_RTIUC1 0x00000034 Memory Mapped
RTI0_RTICPUC1 0x00000000 Memory Mapped
RTI0_RTICAFRC1 0x00000000 Memory Mapped
RTI0_RTICAUC1 0x00000000 Memory Mapped
RTI0_RTICOMP0 0x000589F8 Memory Mapped
RTI0_RTIUDCP0 0x00000001 Memory Mapped
RTI0_RTICOMP1 0x00000000 Memory Mapped
RTI0_RTIUDCP1 0x00000000 Memory Mapped
RTI0_RTICOMP2 0x00000000 Memory Mapped
RTI0_RTIUDCP2 0x00000000 Memory Mapped
RTI0_RTICOMP3 0x00000000 Memory Mapped
RTI0_RTIUDCP3 0x00000000 Memory Mapped
RTI0_RTITBLCOMP 0x00000000 Memory Mapped
RTI0_RTITBHCOMP 0x00000000 Memory Mapped
RTI0_RTISETINT 0x00000003 Memory Mapped
RTI0_RTICLEARINT 0x00000003 Memory Mapped
RTI0_RTIINTFLAG 0x0000000F Memory Mapped
RTI0_RTIDWDCTRL 0x5312ACED Memory Mapped
RTI0_RTIDWDPRLD 0x00000FFF Memory Mapped
RTI0_RTIWDSTATUS 0x00000000 Memory Mapped
RTI0_RTIWDKEY 0x0000A35C Memory Mapped
RTI0_RTIDWDCNTR 0x002DFFFF Memory Mapped
RTI0_RTIWWDRXNCTRL 0x00000005 Memory Mapped
RTI0_RTIWWDSIZECTRL 0x00000005 Memory Mapped
RTI0_RTIINTCLRENABLE 0x05050505 Memory Mapped
RTI0_RTICOMP0CLR 0x00000000 Memory Mapped
RTI0_RTICOMP1CLR 0x00000000 Memory Mapped
RTI0_RTICOMP2CLR 0x00000000 Memory Mapped
RTI0_RTICOMP3CLR 0x00000000 Memory Mapped