Part Number: AM2634-Q1
Other Parts Discussed in Thread: AM2634, SYSCONFIG
Tool/software:
We have a use case where we have developed a real-time control power application on Core 2. This was done much before safe MCALs were published by TI. The application was developed using sys config and using MCU+SDK (drivers) for the AM2634. The developed SW was deployed to hardware and was testing for about a year in the field.
There is now a requirement to include functional safety over this work. For this purpose is there any way we can use MCU+SDK drivers and diagnostics or we absolutely must use MCAL for safe drivers. Our worry is, if we need to use MCAL, then we need to perform all the configuration for peripherals (ADC, PWM's, CMPSS, etc) in EBTresOS for generating MCAL configuration and there may be still a chance that some configuration may be overlooked while porting from sysconfig to EBTresos.
We have a few questions on the same.
1. Is there any possibility that sysconfig data can be fed to EBTresos for configuration setup?
2. Is there a way to determine, besides manual checking of generated configuration in EBTresos matches what was made in sysconfig earlier for achieving the same functionality on the peripheral
3. Does the MCAL support all peripheral features that can be configured via syscfg (especially for ADC, PWM, etc)
4. Does EbTresoS support configuration of all parameters that can be done for sysconfig for ADC, PWM, CMPSS?
5. Can MCU+SDK be used in place of MCAL for safety MCU drivers?
The challenge for us is:
1. While porting from sysconfig for SDK to EbTresos for MCAL we may miss some peripheral setting which may slip into the code and cause potential run time issues
2. We are worried if we begin this port we may hit a blocker if EbTresos would not support a specific register configuration for PWM or ADC that maybe available in sysconfig.
Thanks
Roy