Part Number: TMS570LC4357
Tool/software:
Hi, I am trying to debug my Hercules board using OpenOCD and VSCode and I have run into several problems. The one that is currently blocking me is when trying to load the binary into the board. From openOCSD i get the following debug messages:
Debug: 262 239 command.c:153 script_debug(): command - tms570.cpu invoke-event reset-end
Debug: 263 240 gdb_server.c:400 gdb_log_outgoing_packet(): [tms570.cpu] {1} sending packet: $OK#9a
Debug: 264 245 gdb_server.c:383 gdb_log_incoming_packet(): [tms570.cpu] {1} received packet: X0,0:
Debug: 265 245 gdb_server.c:400 gdb_log_outgoing_packet(): [tms570.cpu] {1} sending packet: $OK#9a
Debug: 266 245 gdb_server.c:375 gdb_log_incoming_packet(): [tms570.cpu] {1} received packet: X0,20:<binary-data-32-bytes>
Debug: 267 245 gdb_server.c:400 gdb_log_outgoing_packet(): [tms570.cpu] {1} sending packet: $OK#9a
Debug: 268 245 gdb_server.c:1679 gdb_write_memory_binary_packet(): addr: 0x0, len: 0x00000020
Debug: 269 245 target.c:2344 target_write_buffer(): writing buffer of 32 byte at 0x00000000
Debug: 270 245 cortex_a.c:2753 cortex_a_write_phys_memory(): Writing memory to real address 0x00000000; size 4; count 8
Debug: 271 245 cortex_a.c:2251 cortex_a_write_cpu_memory(): Writing CPU memory address 0x0 size 4 count 8
Debug: 272 247 cortex_a.c:292 cortex_a_exec_opcode(): exec opcode 0xee160f10
Debug: 273 248 cortex_a.c:292 cortex_a_exec_opcode(): exec opcode 0xee000e15
Debug: 274 250 cortex_a.c:292 cortex_a_exec_opcode(): exec opcode 0xee150f10
Debug: 275 251 cortex_a.c:292 cortex_a_exec_opcode(): exec opcode 0xee000e15
Debug: 276 253 cortex_a.c:292 cortex_a_exec_opcode(): exec opcode 0xee100e15
Debug: 277 256 gdb_server.c:375 gdb_log_incoming_packet(): [tms570.cpu] {1} received packet: X20,3fa0:<binary-data-11-bytes>
Debug: 278 256 gdb_server.c:1493 gdb_error(): Reporting -4 to GDB as generic error
Debug: 279 256 gdb_server.c:400 gdb_log_outgoing_packet(): [tms570.cpu] {1} sending packet: $E0E#ba
Debug: 280 256 gdb_server.c:1679 gdb_write_memory_binary_packet(): addr: 0x20, len: 0x00003fa0
Debug: 281 256 target.c:2344 target_write_buffer(): writing buffer of 16288 byte at 0x00000020
Debug: 282 256 cortex_a.c:2753 cortex_a_write_phys_memory(): Writing memory to real address 0x00000020; size 4; count 4072
Debug: 283 256 cortex_a.c:2251 cortex_a_write_cpu_memory(): Writing CPU memory address 0x20 size 4 count 4072
Debug: 284 259 cortex_a.c:292 cortex_a_exec_opcode(): exec opcode 0xee160f10
Debug: 285 259 server.c:608 sig_handler(): Terminating on Signal 15
which indicate that I was able to write the vector table but failed when trying to write the next. From what I have been able to research, maybe I need to configure a specific target in the openOCD for my exact flash configuration or I need som kind of specific driver to be able to write succesfully to flash. Can someone help?
My launch.json command: