Part Number: MSPM0G3107
Tool/software:
how to write main() into bootloder, i want custom bootloader
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am working on FOTA without bootloader. I write an Application1 code at 0x0000000. This application1 receive data over UART and write into flash at 0x00002000(which is my application2). Now I want to jump from app1 to app2. what are the steps required.
for jumping I am using following code
Hi Sarawati,
See the recommendation in our SDK example code:
static void start_app(uint32_t *vector_table)
{
/* The following code resets the SP to the value specified in the
* provided vector table, and then the Reset Handler is invoked.
*
* Per ARM Cortex specification:
*
* ARM Cortex VTOR
*
*
* Offset Vector
*
* 0x00000000 ++++++++++++++++++++++++++
* | Initial SP value |
* 0x00000004 ++++++++++++++++++++++++++
* | Reset |
* 0x00000008 ++++++++++++++++++++++++++
* | NMI |
* ++++++++++++++++++++++++++
* | . |
* | . |
* | . |
*
* */
/* Reset the SP with the value stored at vector_table[0] */
__asm volatile(
"LDR R3,[%[vectab],#0x0] \n"
"MOV SP, R3 \n" ::[vectab] "r"(vector_table));
/* Set the Reset Vector to the new vector table (Will be reset to 0x000) */
SCB->VTOR = (uint32_t) vector_table;
/* Jump to the Reset Handler address at vector_table[1] */
((void (*)(void))(*(vector_table + 1)))();
}
B.R.
Sal