Part Number: AM263P4-Q1
Tool/software:
Hello,
I'm using SDK 9.2.56.
I am flashing a random length file to OSPI flash using Flash_norOspiWrite() via Flash_write().
static int32_t Flash_norOspiWrite(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len);
In this example, the data I want to flash just happens to be '277545' bytes long. The code divides this into 3 iterative calls of Flash_norOspiWrite() where len is:
131072
131072
15401
On the third call where len is 15401, Flash_norOspiWrite() returns SystemP_FAILURE.
If I force the len to be either 15400 or 15402, Flash_norOspiWrite() returns SystemP_SUCCESS.
There's probably a very good reason why an odd number of bytes fails, please confirm it, but at the very least there seems to be a validation step missing in Flash_norOspiWrite() which would have explicitly informed me that len must be even.