Part Number: MSPM0C1104
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I'm using this device in the 8 pin format and having trouble using the Launch pad as a programmer. I have made my own PCB with some local decoupling, and am trying to program by taking VSS, VDD, SWD, SWD & nRST across to the chip. I continuously get
"CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information. ", but when I monitor the device using scope probes, it programs and runs just fine.
This leads me to believe that SWD/SWC need pullups, but they are not in the schematic of the Launch pad, which programs the on-board 20 pin chip just fine too. the cables are only about 6" long to my target PCB, the programming just seems a bit flaky. Any insights?
Using CCS 20.1.1.8__1.7.1