Part Number: AM263P4-Q1
Other Parts Discussed in Thread: SYSCONFIG, CCSTUDIO, UNIFLASH, AM263P4
Tool/software:
I'm trying to rebuild SBL for a QSPI flash, and was able to read the table using the OSPI Diag example. Tried following the insrtuctions to load the exported JSON file in SysConfig, but it never loads. I turned on the Error Log view in CCS, and it throws this error:
eclipse.buildId=4.23.0.I20220308-0310
java.version=11.0.13
java.vendor=Eclipse Adoptium
BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_CA
Framework arguments: -product com.ti.ccstudio.branding.product
Command-line arguments: -os win32 -ws win32 -arch x86_64 -product com.ti.ccstudio.branding.product
com.ti.ccstudio.project.ui.webcontent
Error
Tue Apr 15 11:53:22 NDT 2025
An internal error was logged by 'com.ti.ccstudio.project.ui.webcontent'.
java.io.IOException: Cannot run program "copy" (in directory "C:\Users\******\AM263P4_WORKSPACE\sbl_jtag_uniflash_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release"): CreateProcess error=2, The system cannot find the file specified
at java.base/java.lang.ProcessBuilder.start(Unknown Source)
at java.base/java.lang.ProcessBuilder.start(Unknown Source)
at com.ti.ccstudio.project.ui.webcontent.internal.sysconfig.BrowserExtensionContribution.spawnCommand(BrowserExtensionContribution.java:1867)
at com.ti.ccstudio.project.ui.webcontent.internal.sysconfig.BrowserExtensionContribution.spawnCommand(BrowserExtensionContribution.java:1823)
at com.ti.ccstudio.project.ui.webcontent.internal.sysconfig.BrowserExtensionContribution.api_spawn(BrowserExtensionContribution.java:1516)
at com.ti.ccstudio.project.ui.webcontent.internal.sysconfig.BrowserExtensionContribution$25.execute(BrowserExtensionContribution.java:593)
at com.ti.browser.internal.TIBrowser$6.execute(TIBrowser.java:381)
at com.ti.chromium.browser.internal.jxbrowser.BrowserFunctionAdapter$1.invoke(BrowserFunctionAdapter.java:53)
at com.teamdev.jxbrowser.js.internal.JsAccessibleObject.invokeAsFunction(JsAccessibleObject.java:218)
at com.teamdev.jxbrowser.js.internal.JsAccessibleObject.invokeMethod(JsAccessibleObject.java:121)
at com.teamdev.jxbrowser.frame.internal.FrameImpl.lambda$processCallback$4(FrameImpl.java:201)
at java.base/java.util.Optional.map(Unknown Source)
at com.teamdev.jxbrowser.frame.internal.FrameImpl.processCallback(FrameImpl.java:201)
at com.teamdev.jxbrowser.internal.rpc.stream.CallbackStream.process(CallbackStream.java:181)
at com.teamdev.jxbrowser.internal.rpc.stream.Stream$StreamObserver.lambda$onNext$0(Stream.java:167)
at com.teamdev.jxbrowser.internal.RpcThreadImpl$TaskRunner.processTasks(RpcThreadImpl.java:172)
at java.base/java.lang.Thread.run(Unknown Source)
Caused by: java.io.IOException: CreateProcess error=2, The system cannot find the file specified
at java.base/java.lang.ProcessImpl.create(Native Method)
at java.base/java.lang.ProcessImpl.<init>(Unknown Source)
at java.base/java.lang.ProcessImpl.start(Unknown Source)
... 17 more
I tried a fresh install on another computer and got the same issue. Am I missing something? Attaching the custom flash JSON file.