Part Number: AM2612
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi, I have the following two question about programming the AM261x uC:-
1) Which programming header is proposed for the PCBA design? what is the protocol? and which pins does it pin to on the AM261…ZEJ variant. The only option I see in SysConfig for this part is JTAG. Note; Usually for ARM uCs I use the ARM single wire protocol via the standard 10pin 1.27mm pitch ARM programming header. Connector pinout pasted below.

2) Which programmer does TI recommend for connection to the programming header and what is the recommended process for programming and debugging?
Thank you