Part Number: MSP432E401Y
Other Parts Discussed in Thread: MSP-EXP432E401Y,
Tool/software:
Hi all,
I’m planning to work with the MSP-EXP432E401Y LaunchPad (based on the MSP432E401Y, ARM Cortex-M4F), and I’m currently exploring the possibility of developing my embedded application using MATLAB/Simulink with Embedded Coder.
I’d appreciate some clarification on the following points:
- Code Generation Support
- Is the MSP-EXP432E401Y officially supported for code generation in Simulink using Embedded Coder?
- I’ve installed Embedded Coder and the Simulink Support Packages for TI C2000 and ARM Cortex-based processors, but I haven’t found a specific hardware target or reference examples for this board.
- Could you suggest the recommended Embedded Coder configuration (e.g., system target file, toolchain, etc.) to generate code for this board?
- Additionally, since MathWorks typically doesn’t generate Code Composer Studio (CCS) projects for ARM processors, what is the suggested workflow for building and debugging the generated code on the MSP432 platform?
- Peripheral Support and Drivers
- Are there any Simulink driver blocks available for peripherals like GPIO, UART, ADC, or Timers for the MSP432E401Y?
- Or is the recommended approach to implement low-level drivers manually in C, and then interface with them using C Caller blocks, S-Functions, or the Legacy Code Tool?
Any guidance or best practices for integrating Simulink-generated code into a CCS-based development workflow would be very helpful.
Thanks in advance for your support,
Pasquale