Part Number: MSPM0L1228
Tool/software:
This is what is stated by the errata I2C_ERR_05:
Function: I2C SDA may get stuck to zero if we toggle ACTIVE bit during ongoing transaction
Description: If ACTIVE bit is toggled during an ongoing transfer, its state machine will be reset. However, the SDA and SCL output which is driven by the master will not get reset. There is a situation where SDA is 0 and master has gone into IDLE state, here the master won't be able to move forward from the IDLE state or update the SDA value. Slave's BUSBUSY is set (toggling of the ACTIVE bit is leading to a start being detected on the line) and the BUSBUSY won't be cleared as the master will not be able to drive a STOP to clear it.
Workaround: Do not toggle the ACTIVE bit during an ongoing transaction.
I am using the I2C peripheral in slave/target mode, and we need to be able to turn off the ACTIVE bit. However, we can't guarantee that we won't be in the middle of a transaction since transactions are initiated by the master/controller.
Does resetting the I2C peripheral via the RSTCTL register cause the SDA line to be released? Or is a full BOOTRST or POR required?
Thanks!