Part Number: TMS570LC4357
Tool/software:
Please confirm below statements are applicable for TMS570LC4357:
a) Frame Check Sequence (FCS) calculation and verification in the MAC (Media Access Control) layer of the TMS570LC4357 is handled at the hardware level.
b) Hardware MAC:
The TMS570LC4357 includes a hardware MAC module, which is responsible for managing the physical layer of the Ethernet communication.
c) FCS Calculation:
The MAC hardware automatically calculates the FCS (also known as the Cyclic Redundancy Check or CRC) for transmitted frames and verifies the FCS for received frames.
Please confirm above information is correct.
Please confirm FCS calculated in microcontroller at hardware level.
Please confirm Ethernet PHY function in microcontroller reject with the incorrect FCS.