Part Number: MSPM0G3105
Tool/software:
Hello TI Community,
I'm encountering a compilation issue with my project for the MSPM0G3105 in CCS. My goal is to use the SDK with the TI Drivers library to program the MSPM0.

However, when I call functions from the ADC.h library, such as ADC_init(), the build process fails. After some testing, I've noticed that the compiler seems to identify errors in the SDK header files (.h) but not in the corresponding source files (.c).
#include <stdbool.h>
#include <stdint.h>
#include <string.h>
#include <stdio.h>
#include "ti_msp_dl_config.h"
#include <ti/drivers/ADC.h>
#define ADC_SAMPLE_COUNT 10
int main(void)
{
SYSCFG_DL_init();
ADC_init();
printf("Hello\n");
return 0;
}
[0]**** Build of configuration Debug for project Dongle_ble **** [1]"D:\\ti\\ccs2011\\ccs\\utils\\bin\\gmake" -k -j 8 all -O [2]Building file: "../Dongle_BLE.c" [3]Invoking: Arm Compiler [4]"D:/ti/ccs2011/ccs/tools/compiler/ti-cgt-armllvm_4.0.2.LTS/bin/tiarmclang.exe" -c @"syscfg/device.opt" -march=thumbv6m -mcpu=cortex-m0plus -mfloat-abi=soft -mlittle-endian -mthumb -O2 -I"D:/Deping/4. Code/Dongle_ble" -I"D:/Deping/4. Code/Dongle_ble/Debug" -I"D:/ti/ccs2011/mspm0_sdk_2_04_00_06/source/third_party/CMSIS/Core/Include" -I"D:/ti/ccs2011/mspm0_sdk_2_04_00_06/source" -gdwarf-3 -MMD -MP -MF"Dongle_BLE.d_raw" -MT"Dongle_BLE.o" -I"D:/Deping/4. Code/Dongle_ble/Debug/syscfg" @"syscfg/device.opt" -o"Dongle_BLE.o" "../Dongle_BLE.c" [5]Finished building: "../Dongle_BLE.c" [6]Building target: "Dongle_ble.out" [7]Invoking: Arm Linker [8]"D:/ti/ccs2011/ccs/tools/compiler/ti-cgt-armllvm_4.0.2.LTS/bin/tiarmclang.exe" @"syscfg/device.opt" -march=thumbv6m -mcpu=cortex-m0plus -mfloat-abi=soft -mlittle-endian -mthumb -O2 -gdwarf-3 -Wl,-m"Dongle_ble.map" -Wl,-i"D:/ti/ccs2011/mspm0_sdk_2_04_00_06/source" -Wl,-i"D:/Deping/4. Code/Dongle_ble/Debug/syscfg" -Wl,-i"D:/ti/ccs2011/ccs/tools/compiler/ti-cgt-armllvm_4.0.2.LTS/lib" -Wl,--diag_wrap=off -Wl,--display_error_number -Wl,--warn_sections -Wl,--xml_link_info="Dongle_ble_linkInfo.xml" -Wl,--rom_model -o "Dongle_ble.out" "./Dongle_BLE.o" "./syscfg/ti_msp_dl_config.o" "./startup_mspm0g310x_ticlang.o" -Wl,-l"syscfg/device_linker.cmd" -Wl,-ldevice.cmd.genlibs -Wl,-llibc.a [9]makefile:137: recipe for target 'Dongle_ble.out' failed [10]warning #10210-D: creating ".sysmem" section with default size of 0x800; use the -heap option to change the default size [11] undefined first referenced [12] symbol in file [13] --------- ---------------- [14] ADC_config D:/ti/ccs2011/mspm0_sdk_2_04_00_06/source/ti/drivers/lib/ticlang/m0p/drivers_mspm0g1x0x_g3x0x.a<ADC.o> [15] ADC_count D:/ti/ccs2011/mspm0_sdk_2_04_00_06/source/ti/drivers/lib/ticlang/m0p/drivers_mspm0g1x0x_g3x0x.a<ADC.o> [16] HwiP_disable D:/ti/ccs2011/mspm0_sdk_2_04_00_06/source/ti/drivers/lib/ticlang/m0p/drivers_mspm0g1x0x_g3x0x.a<ADC.o> [17] HwiP_restore D:/ti/ccs2011/mspm0_sdk_2_04_00_06/source/ti/drivers/lib/ticlang/m0p/drivers_mspm0g1x0x_g3x0x.a<ADC.o> [18]error #10234-D: unresolved symbols remain [19]error #10010: errors encountered during linking; "Dongle_ble.out" not built [20]tiarmclang: error: tiarmlnk command failed with exit code 1 (use -v to see invocation) [21]gmake[1]: *** [Dongle_ble.out] Error 1 [22]makefile:133: recipe for target 'all' failed [23]gmake: *** [all] Error 2 [24]**** Build Finished *
I was wondering if anyone has experienced this type of behavior before and could shed some light on why the compiler doesn't seem to be taking the SDK .c files into account.
Any guidance or suggestions would be greatly appreciated.
Thank you in advance for your help!