Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1227: Interfacing DP83848 with TMS570LS1227

Part Number: TMS570LS1227
Other Parts Discussed in Thread: DP83640, , HALCOGEN

Tool/software:

Hello,

for a custom project I am trying to interface a DP83848 with TMS570LS1227. I chose the DP83848 instead of the DP83640 since it is AEC-Q100 certified.

I never worked before with Ethernet on this chip/mcu and I am trying to find a starting example.

So far, I found the lwip examples on the Texas Instruments git, but it seems it is not working, since I am not able to read the Phy registers such as ID (I am basically stuck inside EMACHWInit.

Some more details about my config:

- I am using RMII mode, COL and RXD2:3 are left floating (but as far as I know they have internal pullups/downs)

- I have a 50MHz oscillator as per Application note describing RMII config with this chip.

- RMII mode enabled in HALCogen, by disabling "Enable MII" under EMAC Tab

Can someone provide me some more infos about the following points?

- should the COL and RXD2:3 pins be fitted with pull ups/downs to be sure a defined PHY address is detected at startup? As a reference, I have configured at startup RXD0:1 pins to be TTL "1" and then I also proceed in pulling TTL"0" on Ethernet reset pin to provide consistency in the bootstrap of the connected pins

- should I change something in the DP83640 c/h file to make it working with DP83848? As I understand basic registers are equal

- IS there any basic example about phy communication with the TMS?

- do you have any specific advice on what to check or understanding why the example is not working ?