Part Number: MSPM0G3507
Tool/software:
Hi,
I have built a traditional CAN communication device that uses an interrupt-based communication method. Separately, I have also set up CAN-FD communication using a broadcast approach. When only one CAN device is communicating via interrupt, the communication works successfully. Similarly, when broadcasting CAN-FD messages alone, communication also works fine. However, when I connect the CAN device and simultaneously continue broadcasting CAN-FD messages, the communication fails.
Below is my fail data through LA

Best Regards,
Andy