This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM261: EPWM generating a different frequency

Part Number: LP-AM261

Tool/software:

Hello,

I was trying to run an SDK example :epwm_hr_duty_cycle_am261x-lp_r5fss0-0_nortos_ti-arm-clang , which is expected to create a 1 khz, 25% duty  EPWM, but while I measure the frequency with 2 different DSO iam getting 1.25khz with 25% dutycycle.

Is this frequency deviation normal? 

  • Hi Adwaith,

    It's due to the R5F clock being 500MHz and SYSCLK at 250MHz, EPWMCLK is directly derived from SYSCLK.

    The expected 1KHz frequency is for 200MHz EPWMCLK.

    Therefore, you are not facing any frequency deviation. You can change the epwm timebase divider values and confirm this.

    I'll file a ticket to mention this in the example!

    Thanks and regards,
    Akshit