Part Number: AM2634
Tool/software:
Hi, experts,
There are Internal Oscillator in AM2634, RCOSC32K and CIO's RCCLK_10M, but the accuracies of them are not mentioned in datasheet. Can you please help to share?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Fan,
Apologies for the late reply.
The RCOSC clock of 10MHz has the below specifications
| Parameter | Min | Nominal | Max | Units |
| Freq(trimmed) | 8 | 10 | 12 | MHz |
| Duty Cycle | 40 | 60 | % | |
| Temperature | -40 | 30 | 150 | °C |
I have reached out to our experts on getting details of RCOSC clock of 32kHz, will let you know once I find the same.
Thanks,
Tejas Kulakarni
Hi Fan,
Please find below the details of RCOSC clock of 32kHz
| Parameter | Min | Nominal | Max | Units |
| Freq(trimmed) | 16 | 32 | 60 | kHz |
| Duty Cycle | 30 | 50 | 70 | % |
| Junction temperature | -40 | 30 | 125 | °C |
Hope these answers give you all the details you were looking for.
Thanks,
Tejas Kulakarni
Hi, Tejas,
Thanks for your reply.
Parameter Min Nominal Max Units Freq(trimmed) 8 10 12 MHz
May I understand the accuracy of 10MHz RCOSC is -20% ~ +20%?
Hi Fan,
accuracy of 10MHz RCOSC is -20% ~ +20%
Yes, that is correct. The accuracy of 10MHz RCOSC is ±20%.
Thanks,
Tejas Kulakarni
Hi Fan,
I have edited the above answers and added the respective temperature details.
Thanks,
Tejas Kulakarni