Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi TI Experts,
For the linux installer of SDK we provided, we support the below options.

Customer could use the --installer-language option to select the language, and using the prefix to select the installation path. However, there is no option to agree the license.
When manually install the linux installer, we need select language, select the installation path, and also agree the license.
Customer is implementing an automatic way to automatically using the Linux command to install the SDK installer. They could 90% achieve this by using --installer-language option & prefix option to input them in the command line, however, since there is no option to agree the license, customer cannot 100% to automatically install the SDK installer using the command line shown below.

Customer is asking if we could add the agree license option in our future SDK Linux installer so that they could eventually install the Linux installer automatically, this is really important for the SDK maintenance from a long term perspective.
Thanks,
Kevin