Part Number: MSPM0C1104
Other Parts Discussed in Thread: BQ40Z50
Tool/software:
Hi
In MSPM0C1104 [ #define I2C_SYS_FENTRIES (4) /* !< Number of FIFO entries */] . SMBUS/I2C TX/RX buffer size is 4 bytes only. And we can not increase this. So we are not able to fill and transmit more than 4 byte data using functions like [DL_I2C_fillControllerTXFIFO],[ DL_I2C_startControllerTransferAdvanced] , [DL_I2C_startControllerTransfer].For flash write/Block write we need more than 4 bytes. I tried many options like below but still it is sending 4 bytes only.
We are using this MCU and functionality with BQ40Z50 R2.
gI2cControllerStatus = I2C_STATUS_IDLE;
gTxLen = count+1;// I2C_TX_PACKET_SIZE;//count+1;//I2C_TX_PACKET_SIZE;
gTxCount = DL_I2C_fillControllerTXFIFO(SMBUS_0_INST, &I2Ctxbuff[0], gTxLen);
/* Enable TXFIFO trigger interrupt if there are more bytes to send */
if (gTxCount < gTxLen) {
DL_I2C_enableInterrupt(SMBUS_0_INST, DL_I2C_INTERRUPT_CONTROLLER_TXFIFO_TRIGGER);
}
else
{
DL_I2C_disableInterrupt(SMBUS_0_INST, DL_I2C_INTERRUPT_CONTROLLER_TXFIFO_TRIGGER);
}
/*
* Send the packet to the controller.
* This function will send Start + Stop automatically.
*/
gI2cControllerStatus = I2C_STATUS_TX_STARTED;
while (!(DL_I2C_getControllerStatus(SMBUS_0_INST) & DL_I2C_CONTROLLER_STATUS_IDLE)) ;
DL_I2C_startControllerTransfer(SMBUS_0_INST, I2C_TARGET_ADDRESS, DL_I2C_CONTROLLER_DIRECTION_TX, gTxLen);
/* Wait until the Controller sends all bytes */
while ((gI2cControllerStatus != I2C_STATUS_TX_COMPLETE) && (gI2cControllerStatus != I2C_STATUS_ERROR))
{
__WFE();
}
while (DL_I2C_getControllerStatus(SMBUS_0_INST) & DL_I2C_CONTROLLER_STATUS_BUSY_BUS)
;
uint32_t status = DL_I2C_getControllerStatus(SMBUS_0_INST);
/* Trap if there was an error */
if (DL_I2C_getControllerStatus(SMBUS_0_INST) &
DL_I2C_CONTROLLER_STATUS_ERROR) {
/* LED will remain high if there is an error */
__BKPT(0);
// if (status & DL_I2C_CONTROLLER_STATUS_NACK)
// printf("NACK received!\n");
if (status & DL_I2C_CONTROLLER_STATUS_ARBITRATION_LOST)
__BKPT(2);
// if (status & DL_I2C_CONTROLLER_STATUS_BUS_ERROR)
// printf("Bus error!\n");
if (status & DL_I2C_CONTROLLER_STATUS_ERROR)
__BKPT(3);
}
while (!(
DL_I2C_getControllerStatus(SMBUS_0_INST) & DL_I2C_CONTROLLER_STATUS_IDLE))
it stops at _BKPT(3); always.