Part Number: MCU-PLUS-SDK-AM243X
Tool/software:
Hello TI Community,
I am currently working with the AM243x LaunchPad and utilizing the M4 core, which has extended only 4 pins dedicated for UART. Given these constraints, I want to configure the SPI peripheral on the M4 core, and I have two potential approaches:
-
Software Emulation: The first approach is to emulate SPI communication through software, which could potentially alleviate the pin limitation issue.
-
MCSPI Peripheral Use: The second idea involves using the MCSPI peripheral available on the M4 core and setting up internal interrupts that connect with the UART pins using the MCSPI registers. My main questions regarding this approach are:
- Is this approach feasible?
- What steps are involved in setting up internal interrupts to route to the UART pins via MCSPI registers?
- What limitations or challenges might I encounter with this method?
Request:
- Detailed guidance on setting up SPI using the MCSPI peripheral with interrupts connecting to UART pins.
- The feasibility of using internal interrupts in this manner, given the hardware constraints.
- Any potential limitations or considerations I should be aware of.
- Resources or documentation that could assist with these configurations.
I appreciate any insights or recommendations from the community to explore these options effectively.
Thank you for your assistance!
Best Regards,
Petr