Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: TMDS243EVM, UNIFLASH
Tool/software:
Hi,
I'm trying to bringup all 4 cores on the TMDS243EVM , but see only two.
I'm using ind_comms_sdk_am243x_09_01_00_03\mcu_plus_sdk.
I've put the EVM into UART boot then used on win cmd:
c://ti/ind_comms_sdk_am243x_09_01_00_03/mcu_plus_sdk/tools\boot>python uart_uniflash.py --cfg=sbl_prebuilt/am243x-evm/default_sbl_null.cfg -p COM6
I've got :
Executing command 2 of 2 ...
Command arguments : --file=sbl_prebuilt/am243x-evm/sbl_null.release.hs_fs.tiimage --operation=flash --flash-offset=0x0
Sent sbl_prebuilt/am243x-evm/sbl_null.release.hs_fs.tiimage of size 293629 bytes in 30.95s.
[STATUS] SUCCESS !!!
All commands from config file are executed !!!
Then I swith to OSPI boot and re-start the board
I get on my UART terminal:
Starting NULL Bootloader ...
DMSC Firmware Version 9.1.6--v09.01.06 (Kool Koala)
DMSC Firmware revision 0x9
DMSC ABI revision 3.1
INFO: Bootloader_runCpu:155: CPU r5f1-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU r5f1-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU m4f0-0 is initialized to 400000000 Hz !!!
INFO: Bootloader_loadSelfCpu:207: CPU r5f0-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_loadSelfCpu:207: CPU r5f0-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runSelfCpu:217: All done, reseting self ...
I see only two CPU's r5f1-0 and r5f1-1.
Which *.cfg is for booting all 4 CPU's ?
Thanks,
Eli.