Part Number: AM2432
Tool/software:
HI TI Extert,
Can you please check and confirm that 'AM2432BSEFHIALVR' operate/RUN without external flash memory?
-
Vaibhav
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2432
Tool/software:
HI TI Extert,
Can you please check and confirm that 'AM2432BSEFHIALVR' operate/RUN without external flash memory?
-
Vaibhav
Hello Vaibahv,
The AM243x does not have any internal flash memories to store the app images.
So, we need the external memories to keep the app images.
When we do POR/WarmReset, the Boot starts from RBL(ROM bootloader) → SBL(Secondary Bootloader) → Application (DDR/MSRAM).
Here, the SBL will take the app images from the external memories and put them into the DDR /MSRAM memory.
And, now the Application runs from DDR/MSRAM memory.
Regards,
Anil.
Dear Anil,
Thank you for your guidance.
Could you please provide further clarification on the following points?
In the case where the AM243x device does not have external memories, is it possible to boot the device from USB and run the application on AM243x?
Could you kindly check and confirm whether the 'AM2432BSEFHIALVR' can operate/run without external DDR memory?
Looking forward to your response.
Best regards,
Vaibhav
Hello Vaibhav,
The AM243X has internal memory of up to 2MB and in which some memory is used for DM (Device Management ) operations .
So, if your application is less than 2MB, then go ahead and use the AM243X device without DDR.
In the case where the AM243x device does not have external memories, is it possible to boot the device from USB and run the application on AM243x?
This is not possible. We need to keep the app images in external memory. Otherwise, even if we write app images on the MSRAM/DDR memory, after the reset the DDR/MSRAM content will be lost. Then again, the R5F core runs from which location ?
So, we have to keep app images in external memory. Please read the chapter below to understand better SBL and memory layout.
Regards,
Anil.