Tool/software:
Hello @all,
I have a question about the timer capture!
How can I configure this timer correctly on the controller (MSPM03507)?
How can I correctly configure the timer on the controller (MSPM03507) that you see in the picture below?

In the next picture is my configuration in CCS12.8.1. the problem is that this configuration uses 3 timers.
I need 1 timer with 3 inputs.
How do I set this, if this is possible?