This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: EnDat: Multiple encoder with different resolution

Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hi experts,

We would like to connect two different EnDat encoders to the controller, which differ in singleturn and multiturn resolution.

Although both encoders are initialized correctly and the resolution can be read out correctly, there seems to be a bug in the driver interface.

The driver interface only stores the position resolution of the most recently initialized encoder, which is then used in endat_recvd_process() for all encoders. Therefore, the received position bytes are misinterpreted for all encoders except the most recent one.

It would be great if you could check on this issue. Let me know if you need additional information about my setup!

Thanks and regards,
Stefan