Part Number: MSPM0G3519
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi, I have a question about the FRANGE setting. In all the examples I see:
SYSCONFIG_WEAK void SYSCFG_DL_SYSCTL_init(void)
{
//Low Power Mode is configured to be SLEEP0
DL_SYSCTL_setBORThreshold(DL_SYSCTL_BOR_THRESHOLD_LEVEL_0);
DL_SYSCTL_setSYSOSCFreq(DL_SYSCTL_SYSOSC_FREQ_BASE);
/* Set default configuration */
DL_SYSCTL_disableHFXT();
DL_SYSCTL_disableSYSPLL();
DL_SYSCTL_setULPCLKDivider(DL_SYSCTL_ULPCLK_DIV_1);
DL_SYSCTL_setMCLKDivider(DL_SYSCTL_MCLK_DIVIDER_DISABLE);
}
static const DL_ADC12_ClockConfig gADC12_0ClockConfig = {
.clockSel = DL_ADC12_CLOCK_ULPCLK,
.divideRatio = DL_ADC12_CLOCK_DIVIDE_8,
.freqRange = DL_ADC12_CLOCK_FREQ_RANGE_24_TO_32,
};
Shouldn't the FRANGE setting be DL_ADC12_CLOCK_FREQ_RANGE_4_TO_8?