Tool/software:
Hi,
As the title states the latest Code Composer Studio v20.1.1 says that it cannot detect any compatible board.
More specifically in the Get Started tab that opens up as soon as you start CCS it says: "No compatible board detected - please connect your board".
The board is connected to the PC and powered by the recommended 12V power supply.
In the Device Manager I can see both entries under the Texas Instruments Debug Probes (XDS110 Class Data Port , XDS110 Class Debug Probe) and under the Ports (XDS110 Class Application/User UART , XDS110 Class Auxiliary Data Port).
There are 2 jumpers placed on the SOP0 and SOP1 positions to enter NOBOOT mode.
The JTAG_MUX switch is also set to the XDS position.
The evaluation board is also REV. C if that plays any role.
Is there anything I am missing?
If you need any further information please let me know.
Best regards,
Konstantinos Skyvalakis