Part Number: TMS470MF06607
Tool/software:
S4MF06607BSPZQQ1, D/C:2340+5, 2342, 2345+5,
L/N:4009456PHI, 3599770PHI, 3627159PHI, 3627165PHI,
COO:PH, MSD PKG, ROHS, ST
The Controler has failed in the EOL Test. Image is attached for your reference.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS470MF06607
Tool/software:
S4MF06607BSPZQQ1, D/C:2340+5, 2342, 2345+5,
L/N:4009456PHI, 3599770PHI, 3627159PHI, 3627165PHI,
COO:PH, MSD PKG, ROHS, ST
The Controler has failed in the EOL Test. Image is attached for your reference.
HI,
What is your EOL test?
Is this part of your production test?
What exactly has failed?
Has this unit been on the field yet?
Hi,
I have not heard back from you. I will close the thread for now. If you have any update you can write back to this post and the status will change to OPEN.
What is your EOL test? :- End of line testing it is our final testing stage
Is this part of your production test? Yes
What exactly has failed? :- VCU was not communicated (no signal) with our Electronic box
Has this unit been on the field yet? :- No its got defected at customer end of line testing
What exactly has failed? :- VCU was not communicated (no signal) with our Electronic box
Hi,
What type of communication is used (e.g. UART, SPI or etc)?
Can you show a probe capture of the signals on a known good board vs the failure board?
On the failure board, can you toggle these pins as in GPIO mode?
Can you do a ABA swap test? Will failure follow the MCU?
The A-B-A Swap Method is a simple cross check test, which can confirm the observed issue is not systemic.