Part Number: TMS570LC4357
Tool/software:
I have initialized the ADC module in the TI Hercules TMS570LC43xx with a 12-bit resolution.
When I provide an external input to the microcontroller to test the ADC, I am getting a count of 4095 at 3.1V (external input to the controller).
What could be the problem?
I have the jumper ON at J8 on the development board, which enables 3.3V to the ADC.