Part Number: AM263P4-Q1
Tool/software:
Hi Team,
It says the following in the CAN SDK documentation:
- The Busoff state is reported by setting PSR.BO.
Can you advise on how SDK APIs should be used configure PSR.BO such that it will detect Busoff?
- What SDK API should be used to detect Busoff state?
- What SDK API should be used to recover from detected Busoff state?
They want to use polling method instead of interrupt.
It also says to do below:
- To restart CAN operation, the application software needs to clear CCCR.INIT.
Can you advise on how to do this and what else needs to be done?
- After CCCR.INIT is configured through HW, is the only step necessary to restart CAN operation to clear CCCR.INIT?
- What SDK API should be used to clear CCCR.INIT? How should they use this?
- After clearing CCCR.INIT, do the CAN settings remain as configured previously? (ie. ID filter and FIFO settings)
Best regards,
Mari Tsunoda