Part Number: MSPM0G1106
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
We are currently trying to implement a MSPM0G1106 into our design. The device is connected via I2C with our main MCU.
We are using MSPM0 SDK 2.4.0.06, SysConfig 1.21.1 and TI-clang 4.0.2 LTS.
We are required to change the I2C address for the BSL since there's already another bus device using the default I2C address of 0x48.
We also want to read the application version via the BSL requiring us to set the corresponding values in the configuration NVM.
We have the following settings in our sysconfig:
NONMAIN.nonmainWarning = true; NONMAIN.bslAppVersion = 0xC0; NONMAIN.i2cSlaveAddress = 0x50;
Flashing the device via our J-Link seems to work fine once but after attempting a 2nd flash the flash fails and results in the device being complete unresponsive. Only the application code was changed for the 2nd flash, the BSL config hasn't been changed.
The following error is reported during flashing:
CORTEX_M0P: Trouble Writing Memory Block at 0x41c00100 on Page 0 of Length 0x58: Flash download failed! ... CORTEX_M0P: File Loader: Verification failed: Target failed to write 0x41C00100 CORTEX_M0P: GEL: File: XXXXXXXXXXX.out: Load failed.
Now only the following is reported when attempting to connect to the device:
Device "MSPM0G1106" selected. Connecting to target via SWD Found SW-DP with ID 0x6BA02477 DPIDR: 0x6BA02477 CoreSight SoC-400 or earlier Scanning AP map to find all available APs AP[0]: Stopped AP scan as end of AP map has been reached Iterating through AP map to find AHB-AP to use Attach to CPU failed. Executing connect under reset. DPIDR: 0x6BA02477 CoreSight SoC-400 or earlier Scanning AP map to find all available APs AP[0]: Stopped AP scan as end of AP map has been reached Iterating through AP map to find AHB-AP to use Could not find core in Coresight setup Found SW-DP with ID 0x6BA02477 DPIDR: 0x6BA02477 CoreSight SoC-400 or earlier Scanning AP map to find all available APs AP[0]: Stopped AP scan as end of AP map has been reached Iterating through AP map to find AHB-AP to use Attach to CPU failed. Executing connect under reset. DPIDR: 0x6BA02477 CoreSight SoC-400 or earlier Scanning AP map to find all available APs AP[0]: Stopped AP scan as end of AP map has been reached Iterating through AP map to find AHB-AP to use Could not find core in Coresight setup Cannot connect to target.
Trying to use the DSSM Factory reset tool with a XDS110 doesn't work. Neither do the JlinkScripts from this thread e2e.ti.com/.../mspm0l1305-dssm-commands-to-factory-reset-without-xds110 with our J-Link.
This happened with 2 out of 2 devices.
While I do understand that misconfiguring the NONMAIN region may brick the device I'm a bit confused to why it is happening in this instance.
Are we missing something? Is there any chance to recover the devices?