Part Number: MSPM0L1227-Q1
Tool/software:
Dear team,
I am performing flash read at Address "0x0001F000" as below. Write opration is successful and I can see the intended data in memory window.
Code snippet from write API,
DL_FlashCTL_executeClearStatus(FLASHCTL);
DL_FlashCTL_unprotectSector(FLASHCTL, address, DL_FLASHCTL_REGION_SELECT_MAIN);
/* Erase sector in main memory */
gCmdStatus = DL_FlashCTL_eraseMemoryFromRAM( FLASHCTL, address, DL_FLASHCTL_COMMAND_SIZE_ONE_WORD);
/* Ensure proper flash command execution by clearing the STATCMD
* register before executing a flash operation*/
DL_FlashCTL_executeClearStatus(FLASHCTL);
/* 8-bit write to flash in main memory without ECC */
gCmdStatus = DL_FlashCTL_programMemoryFromRAM(FLASHCTL, address, (uint32_t*)data, dataSize, DL_FLASHCTL_REGION_SELECT_MAIN);
if(gCmdStatus == DL_FLASHCTL_COMMAND_STATUS_PASSED)
{
retVal = true;
}
However when I perform flash read operation during next cycle using memcopy/pointer , software does not run anymore. Do I need to take care of some specific steps ?
Code snippet from read API,
uint32_t *EolDataRead = (uint32_t*)0x0001F000;
uint32_t HuberEolDataReadRam = 0;
HuberEolDataReadRam = *HuberEolDataRead;
Regards,
Halappa