Just out of curiosity and for general forum knowledge I have two questions regarding the new I2C peripheral and ETM instruction trace availability in the new LM4F 64-pin devices (i.e. LM4F231E5QR).
When reviewing the Differences Among Stellaris Product Classes (Rev. A), specifically in the I2C section (pg. 16), there is mention of a high-speed mode (Fast-mode plus 1Mbps?) in the Blizzard (LM4F) devices but I can't find any reference to such a mode in the Stellaris LM4F231E5QR Microcontroller Data Sheet. Is this high-speed mode actually present in the LM4F devices but the I2C peripheral documentation has not been updated to reflect such a mode?
Will the 64-pin LM4F devices support the ETM instruction trace port? It appears that 3 of the 4 trace data lines (TRD0, TRD1, and TRD2) as well as trace clock (TRCLK) are allocated in signal tables (pg. 1308) of Stellaris LM4F231E5QR Microcontroller Data Sheet but trace data line 4 (TRD3) appears to be missing. Is this simply a data sheet omission or is ETM not supported on the 64-pin devices?
Thanks,
Jesse Griggs