Part Number: BP-AM2BLDCSERVO
Other Parts Discussed in Thread: LP-AM243, MCU-PLUS-SDK-AM243X
Tool/software:
I'm trying to run Tamagawa Diagnostic using the combination of LP-AM243, BP-AM2BLDCSERVO, and a Tamagawa encoder, as described on this web page.
However, all the commands shown in the console result in a "CRC Failure" message, and it doesn't seem to be working correctly.
For example, when I send the command “0 : Data readout, Absolute (Data ID 0)”, the signals on DATA+ and DATA– are output as shown in the waveform shown below.
Looking at the diagram in “Hardware Setup of Booster Pack + LP for Tamagawa” it appears that the system operates using a 2-wire RS-485 connection for DATA+ and DATA–. In that case, shouldn't J24 be set to ON instead of OFF?
I'm using the following SDK versions:
- MCU-PLUS-SDK-AM243X: 11.00.00.15
- MOTOR-CONTROL-SDK-AM243X: 09.02.00.09
If there are any specific settings or configurations I should check to ensure proper operation, I would appreciate your guidance.
Shinsuke