This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H4010-SEP: BIAS Pin Configuration for Sequential Powering with TPS7H4010-SEP

Part Number: TPS7H4010-SEP

Tool/software:

Hello,

I plan to use two TPS7H4010-SEP devices in a sequential powering configuration. The first IC will have Vout = 1.2V, and its PGood output will be connected to the EN pin of the second IC, which has Vout = 3.3V.

According to the datasheet, the BIAS pin can be tied to a 3.3V or 5V power rail to improve efficiency. My question is: Can I connect the BIAS pin of the 1.2V IC to the 3.3V rail, even though the 3.3V IC will power on only after the 1.2V IC?