Part Number: AM2634-Q1
Tool/software:
Dear TI Support,
I am working on a Battery Management System (BMS) design and using the AM2634-Q1 microcontroller. I am quite new to hardware system design, so I would really appreciate your guidance.
I need to interface the AM2634-Q1's GPMC (General-Purpose Memory Controller) interface to a PC/104-based peripheral. Could you please help me understand: -
1. How can I connect the GPMC interface to a PC/104 bus system?
2. Is GPMC compatible with standard PC/104 (ISA or PCI) signals?
3. Do I need a bridge or additional logic between GPMC and PC/104?
4. Are there any reference designs, application notes, or guidelines?
5. What are the signal voltage levels on GPMC, and do I need level shifting to meet PC/104 specifications?
6. How do I configure the GPMC in the AM2634-Q1 to operate in a mode compatible with memory-mapped peripherals like those used on PC/104 boards?
7. Is there software/driver support in the SDK or MCU+ SDK to access PC/104 peripherals via GPMC?
8. Any TI recommendations for interfacing with legacy parallel buses like PC/104 or ISA using modern MCUs like the AM2634-Q1?
9. Are there any limitations or risks (electrical or timing-wise) that I should be aware of when trying to achieve this communication?