This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634-Q1: Requesting suggestions to resolve issue related to - DMA triggered continuously by ECAP

Part Number: AM2634-Q1

Tool/software:

Hi TI,

I have set up an ECAP to trigger a DMA transfer upon EVENT 2.... and I want the DMA to be triggered continuously as long as ECAP detects EVENT 2 on a signal.
However, I see the DMA being triggered only once. 

Here are my observations during test - 
As soon as I start running code, I see 40 samples of ECAP CAPTURE 2 timestamps stored in measAPWM.buffer. Later when I change the duty cycle on the signal, I don't see the updated duty cycle captured in measAWPM.buffer thus signaling that no DMA transfer occurred after the first transfer.

TPCC_ER remains 0
TPCC_ERR is set to 1
TPCC_EMR is 0
TPCC_IPR is set to 1, however when I write TPCC_ICR = 1, TPCC_IPR is not getting cleared.

The signal is sent at 400KHz frequency.
I would really appreciate your help in resolving this issue at the earliest.
I had also written about this issue in another thread many days ago but haven't seen any response yet.

e2e.ti.com/.../5822122



Below is my PaRAM set up -

  • Hi,

    The ECAP_EDMA example project in the SDK transfers the contents of ECAP capture registers upon ECAP events to pwmTrigTimeStamps and capTrigTimeStamps buffers for 1 parameter set (4*2*256 and 4*4*128 respectively).

    I modified the code to set up this example project to continuously update the buffers. Below is the modified code. However, even in this case, the continuous transfer did not happen. 
    Here are my observations from testing -
    1) Upon executing EDMA_enableTransferRegion() APIs, the first DMA transfer happened and the buffers were filled with ECAP timestamps.
    2) TPCC_IPR was set to 3
    3) Executing EDMA_clrIntrRegion() did not clear TPCC_IPR.
    4) The buffers were updated with 0. 
    5) DMA transfer from ECAP capture registers to buffers did not happen after that as the buffers remained 0. TPCC_IPR remained set to 3 and EDMA_clrIntrRegion() did not clear the TPCC_IPR and this loop continued with no updates to the buffer.

    This is a similar behavior I have observed in my project too.
    Could you please tell me how to set up for continuous transfer?

    I am looking to set up following transfer --> ECAP capture 2 register (4 bytes) is my source address. An array of 40 elements (4 bytes each) is my destination. Every capture 2 event transfers the timestamp to destination buffer via DMA...thus capturing 40 event timestamps in 40 elements of the buffer array. Then the 41st ECAP event should store the timestamp in buffer[0]... and this loop should continue as long as the ECAP events are captured.

    Thanks!

  • /*
     *  Copyright (C) 2021 Texas Instruments Incorporated
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    //
    // Included Files
    //
    #include <kernel/dpl/DebugP.h>
    #include <kernel/dpl/SemaphoreP.h>
    #include <kernel/dpl/HwiP.h>
    #include "ti_drivers_config.h"
    #include "ti_drivers_open_close.h"
    #include "ti_board_open_close.h"
    
    
    /**
     * Example Description:
     *  This example demostrates the ECAP triggerring EDMA for transfer of the ECAP
     * timestamp registers to the TCM location without R5 intervention.
     *
     *  ECAP can generate EDMA triggers for Data transfer in both CAPTURE mode and
     * APWM mode
     * - In ECAP Capture Mode, the CAPEVTx [x= 1 to 4] can be used and
     * - In ECAP APWM Mode, The counter match to Compare or Period can be used.
     *
     *  An ECAP (APWM_ECAP) is configured in APWM mode to generate trigger at
     * its counter matching period event to transfer timestamp data from "CAPTURE_ECAP2".
     * 2 ECAPs (CAPTURE_ECAP1, CAPTURE_ECAP2) are configured to capture the APMW_ECAP PWM
     * wave. CAPTURE_ECAP1 also triggers EDMA on one of its Capture events.
     *
     * ECAP Configurations:
     * 1. APWM_ECAP:
     * - APWM mode, 5KHz and 25% duty cycle
     * - DMA trigger at Counter = Period event for channel 0
     * - Output routed via Outputxbar13 (GPIO119)
     *
     * 2. CAPTURE_ECAP1:
     * - CAPTURE MODE, capturing Falling, Rising, Falling, Rising edges on its four events,
     * - counter resets at CAPEVT1,2,3,4. Thereby, recording
     *      - ON time at CAP1, CAP3,
     *      - OFF times at CAP2,CAP4,
     * - CAPEVT4 is the source for the DMA channel 1 trigger for the transfer of its timestamps in CAPx
     *
     * 3. CAPTURE_ECAP2:
     * - CAPTURE mode, Capturing Falling, Rising edges on its 2 events,
     * - counter resets on CAPEVT1,2. thereby recording,
     *      - ON time on CAP1
     *      - OFF time on CAP2
     *
     *  A total of 256 transfers on Channel 0 and 128 transfers on Channel 1 are triggered,
     * and the buffers "capTrigTimeStamps" and "pwmTrigTimeStamps" are compared.
     *
     * Watch Variables :
     * 1. capTrigTimeStamps [ ]: array with CAPTURE_ECAP1 Captured timestamps, triggered by Capture mode.
     * 2. pwmTrigTimeStamps [ ]: array with CAPTURE_ECAP2 Captured timestamps, triggered by APWM mode.
     *
     * External Connections : No external connections are required.
     *
     */
    
    #define APP_NUM_EDMA_PARAMS (2)
    #define APP_NUM_EDMA_CHANNELS (2)
    
    #define APP_NUM_APWM_TRIG_TRANSFERS (256)   // Each Transfer is of 2 regs
    #define APP_NUM_APWM_TRIG_REG_TRANSFER (2)
    
    #define APP_NUM_CAP_TRIG_TRANSFERS  (128)   // Each Transfer is of 4 regs
    #define APP_NUM_CAP_TRIG_REG_TRANSFER (4)
    
    #define APP_EDMA_A_COUNT (4)    // 4 bytes, 1 in each register
    
    #define EDMA_TEST_EVT_QUEUE_NO_0 (0)    // tptc 0
    
    uint32_t gEdmaPaRams[APP_NUM_EDMA_PARAMS];
    uint32_t gEdmaChannels[APP_NUM_EDMA_CHANNELS] = {
        DMA_TRIG_XBAR_EDMA_MODULE_0,
        DMA_TRIG_XBAR_EDMA_MODULE_1,
    };
    
    uint32_t gEdmaBase, gEdmaRegId, gEdmaTcc[APP_NUM_EDMA_CHANNELS];
    
    uint32_t gApwmEcapBase = APWM_ECAP0_BASE_ADDR;
    uint32_t gCap1EcapBase = CAPTURE_ECAP1_BASE_ADDR;
    uint32_t gCap2EcapBase = CAPTURE_ECAP2_BASE_ADDR;
    
    /* (APP_NUM_CAP_TRIG_TRANSFERS * APP_NUM_CAP_TRIG_REG_TRANSFER)
        or
       (APP_NUM_APWM_TRIG_TRANSFERS * APP_NUM_APWM_TRIG_REG_TRANSFER) */
    #define ARRAY_SIZE (APP_NUM_CAP_TRIG_TRANSFERS * APP_NUM_CAP_TRIG_REG_TRANSFER)
    
    volatile uint32_t capTrigTimeStamps[ARRAY_SIZE] = {0};
    volatile uint32_t pwmTrigTimeStamps[ARRAY_SIZE] = {0};
    
    void App_edmaConfig(void);
    
    void App_edmaDeConfig(void);
    
    bool App_compareInRange(uint32_t input1, uint32_t input2, uint32_t error_range);
    
    void ecap_edma_main(void *args)
    {
    
        bool status = true;
        Drivers_open();
        Board_driversOpen();
    
    
        DebugP_log("ECAP triggered EDMA transfers Test Started ...\r\n");
    
        /* stopping counters for the other configurations */
        ECAP_stopCounter(gApwmEcapBase);
        ECAP_stopCounter(gCap1EcapBase);
        ECAP_stopCounter(gCap2EcapBase);
    
        /* configuring the edma transfers */
        App_edmaConfig();
        /* clearing the interrupts for the edma channel transfer */
        EDMA_clrIntrRegion(gEdmaBase, gEdmaRegId, gEdmaTcc[0]);
        EDMA_clrIntrRegion(gEdmaBase, gEdmaRegId, gEdmaTcc[1]);
    
        /* starting the ECAP counters for the APWM generation and the Captures */
        ECAP_startCounter(gApwmEcapBase);
        ECAP_startCounter(gCap1EcapBase);
        ECAP_startCounter(gCap2EcapBase);
    
        /* enabling the edma transfers */
        EDMA_enableTransferRegion(gEdmaBase, gEdmaRegId, gEdmaChannels[0], EDMA_TRIG_MODE_EVENT);
        EDMA_enableTransferRegion(gEdmaBase, gEdmaRegId, gEdmaChannels[1], EDMA_TRIG_MODE_EVENT);
    
        /* wait while the transfers are complete */
        for(;;)
        {
            for(;;)
            {
                if(
                    (EDMA_readIntrStatusRegion(gEdmaBase, gEdmaRegId, gEdmaTcc[0]) == 1) &&
                    (EDMA_readIntrStatusRegion(gEdmaBase, gEdmaRegId, gEdmaTcc[1]) == 1)
                )
                {
                    break;
                }
            }
    
            EDMA_clrIntrRegion(gEdmaBase, gEdmaRegId, gEdmaTcc[0]);
            EDMA_clrIntrRegion(gEdmaBase, gEdmaRegId, gEdmaTcc[1]);
            for(int i = 0; i<ARRAY_SIZE; i++)
            {
                capTrigTimeStamps[i] = 0;
                pwmTrigTimeStamps[i] = 0;
            }
        }
    
        /* transfers complete. stopping the counters */
    //    ECAP_stopCounter(gApwmEcapBase);
    //    ECAP_stopCounter(gCap1EcapBase);
    //    ECAP_stopCounter(gCap2EcapBase);
    
        /* clearing the EDMA interrupts */
    
    
        DebugP_log("EDMA transfers complete.\r\n");
    
        /* comparing the copied Timestamp registers */
        for(int iter = 0; iter <ARRAY_SIZE; iter++)
        {
            uint32_t error_range = 5;
            status = App_compareInRange(capTrigTimeStamps[iter], pwmTrigTimeStamps[iter], error_range);
            if(status == false)
            {
                DebugP_log("Fail : Copied registers are not in sync | index : %d : cap1 : %d\t cap2 : %d\r\n", iter, capTrigTimeStamps[iter], pwmTrigTimeStamps[iter]);
                status = false;
                break;
            }
            if((capTrigTimeStamps[iter] == 0) || (pwmTrigTimeStamps[iter] == 0))
            {
                DebugP_log("DMA transfer failed\r\n");
                status = false;
                break;
            }
        }
        if(status == true)
        {
            DebugP_log("ECAP triggered EDMA transfers Passed!!\r\n");
            DebugP_log("All tests have passed!!\r\n");
        }
        else
        {
            DebugP_log("ECAP triggered EDMA transfers Failed!!\r\n");
            DebugP_log("Some tests have Failed!!\r\n");
        }
    
        /* deconfiguring the EDMA */
        App_edmaDeConfig();
    
        Board_driversClose();
        Drivers_close();
    }
    
    void App_edmaConfig(void)
    {
        int32_t status = SystemP_SUCCESS;
        EDMACCPaRAMEntry edma_paramEntry;
    
        gEdmaBase = EDMA_getBaseAddr(gEdmaHandle[0]);
        DebugP_assert( gEdmaBase != 0);
    
        gEdmaRegId = EDMA_getRegionId(gEdmaHandle[0]);
        DebugP_assert(gEdmaRegId < SOC_EDMA_NUM_REGIONS);
    
        for(int channel = 0; channel < APP_NUM_EDMA_CHANNELS; channel++)
        {
            status = EDMA_allocDmaChannel(gEdmaHandle[0], &(gEdmaChannels[channel]));
            DebugP_assert(status == SystemP_SUCCESS);
        }
    
        for(int param = 0; param < APP_NUM_EDMA_PARAMS; param++)
        {
            gEdmaPaRams[param] = EDMA_RESOURCE_ALLOC_ANY;
            status = EDMA_allocParam(gEdmaHandle[0], &(gEdmaPaRams[param]));
            DebugP_assert(status == SystemP_SUCCESS);
        }
    
        for(int tcc = 0; tcc < APP_NUM_EDMA_PARAMS; tcc++)
        {
            gEdmaTcc[tcc] = EDMA_RESOURCE_ALLOC_ANY;
            status = EDMA_allocTcc(gEdmaHandle[0], &gEdmaTcc[tcc]);
            DebugP_assert(status == SystemP_SUCCESS);
        }
        /* param set population for the cap triggered transfers */
        EDMA_ccPaRAMEntry_init(&edma_paramEntry);
        edma_paramEntry.srcAddr       = (uint32_t) SOC_virtToPhy((void *)(gCap2EcapBase + CSL_ECAP_CAP1));
        edma_paramEntry.destAddr      = (uint32_t) SOC_virtToPhy((void *) pwmTrigTimeStamps);
        edma_paramEntry.aCnt          = (uint16_t) (APP_EDMA_A_COUNT);
        edma_paramEntry.bCnt          = (uint16_t) (APP_NUM_APWM_TRIG_REG_TRANSFER);
        edma_paramEntry.cCnt          = (uint16_t) (APP_NUM_APWM_TRIG_TRANSFERS);
        edma_paramEntry.bCntReload    = 0;
        edma_paramEntry.srcBIdx       = (int16_t) EDMA_PARAM_BIDX(APP_EDMA_A_COUNT);
        edma_paramEntry.destBIdx      = (int16_t) EDMA_PARAM_BIDX(APP_EDMA_A_COUNT);
        edma_paramEntry.srcCIdx       = (int16_t) 0;
        edma_paramEntry.destCIdx      = (int16_t) APP_EDMA_A_COUNT*APP_NUM_APWM_TRIG_REG_TRANSFER;
        edma_paramEntry.linkAddr      = 0xFFFFU;
        edma_paramEntry.srcBIdxExt    = (int8_t) EDMA_PARAM_BIDX_EXT(0);
        edma_paramEntry.destBIdxExt   = (int8_t) EDMA_PARAM_BIDX_EXT(0);
        edma_paramEntry.opt           = (EDMA_OPT_TCINTEN_MASK | EDMA_OPT_SYNCDIM_MASK |
                                  ((((uint32_t)(gEdmaTcc[0])) << EDMA_OPT_TCC_SHIFT) & EDMA_OPT_TCC_MASK));
    
        EDMA_setPaRAM(gEdmaBase, gEdmaPaRams[0], &edma_paramEntry);
    
        EDMA_ccPaRAMEntry_init(&edma_paramEntry);
        edma_paramEntry.srcAddr       = (uint32_t) SOC_virtToPhy((void *)(gCap1EcapBase + CSL_ECAP_CAP1));
        edma_paramEntry.destAddr      = (uint32_t) SOC_virtToPhy((void *) capTrigTimeStamps);
        edma_paramEntry.aCnt          = (uint16_t) (APP_EDMA_A_COUNT);
        edma_paramEntry.bCnt          = (uint16_t) (APP_NUM_CAP_TRIG_REG_TRANSFER);
        edma_paramEntry.cCnt          = (uint16_t) (APP_NUM_CAP_TRIG_TRANSFERS);
        edma_paramEntry.bCntReload    = 0;
        edma_paramEntry.srcBIdx       = (int16_t) EDMA_PARAM_BIDX(APP_EDMA_A_COUNT);
        edma_paramEntry.destBIdx      = (int16_t) EDMA_PARAM_BIDX(APP_EDMA_A_COUNT);
        edma_paramEntry.srcCIdx       = (int16_t) 0;
        edma_paramEntry.destCIdx      = (int16_t) APP_EDMA_A_COUNT * APP_NUM_CAP_TRIG_REG_TRANSFER;
        edma_paramEntry.linkAddr      = 0xFFFFU;
        edma_paramEntry.srcBIdxExt    = (int8_t) EDMA_PARAM_BIDX_EXT(0);
        edma_paramEntry.destBIdxExt   = (int8_t) EDMA_PARAM_BIDX_EXT(0);
        edma_paramEntry.opt           = (EDMA_OPT_TCINTEN_MASK | EDMA_OPT_SYNCDIM_MASK |
                                  ((((uint32_t)(gEdmaTcc[1])) << EDMA_OPT_TCC_SHIFT) & EDMA_OPT_TCC_MASK));
    
        EDMA_setPaRAM(gEdmaBase, gEdmaPaRams[1], &edma_paramEntry);
    
    
    
    
    
    //    EDMACCPaRAMEntry   edmaParam1,edmaParam2;
    //    uint32_t           param0, param1;
    //
    //    param0 = EDMA_RESOURCE_ALLOC_ANY;
    //    EDMA_allocParam(gEdmaHandle[0], &param0);
    //
    //    param1 = EDMA_RESOURCE_ALLOC_ANY;
    //    EDMA_allocParam(gEdmaHandle[0], &param1);
    //
    //    /* param set population for the cap triggered transfers */
    //    EDMA_ccPaRAMEntry_init(&edmaParam1);
    //    edmaParam1.srcAddr       = (uint32_t) SOC_virtToPhy((void *)(gCap2EcapBase + CSL_ECAP_CAP1));
    //    edmaParam1.destAddr      = (uint32_t) SOC_virtToPhy((void *) pwmTrigTimeStamps);
    //    edmaParam1.aCnt          = (uint16_t) (APP_EDMA_A_COUNT);
    //    edmaParam1.bCnt          = (uint16_t) (APP_NUM_APWM_TRIG_REG_TRANSFER);
    //    edmaParam1.cCnt          = (uint16_t) (APP_NUM_APWM_TRIG_TRANSFERS);
    //    edmaParam1.bCntReload    = 0;
    //    edmaParam1.srcBIdx       = (int16_t) EDMA_PARAM_BIDX(APP_EDMA_A_COUNT);
    //    edmaParam1.destBIdx      = (int16_t) EDMA_PARAM_BIDX(APP_EDMA_A_COUNT);
    //    edmaParam1.srcCIdx       = (int16_t) 0;
    //    edmaParam1.destCIdx      = (int16_t) APP_EDMA_A_COUNT*APP_NUM_APWM_TRIG_REG_TRANSFER;
    //    edmaParam1.linkAddr      = 0xFFFFU;
    //    edmaParam1.srcBIdxExt    = (int8_t) EDMA_PARAM_BIDX_EXT(0);
    //    edmaParam1.destBIdxExt   = (int8_t) EDMA_PARAM_BIDX_EXT(0);
    //    edmaParam1.opt           = (EDMA_OPT_TCINTEN_MASK | EDMA_OPT_SYNCDIM_MASK |
    //                              ((((uint32_t)(gEdmaTcc[0])) << EDMA_OPT_TCC_SHIFT) & EDMA_OPT_TCC_MASK));
    //
    //    EDMA_setPaRAM(gEdmaBase, param0, &edmaParam1);
    //
    //    EDMA_ccPaRAMEntry_init(&edmaParam2);
    //    edmaParam2.srcAddr       = (uint32_t) SOC_virtToPhy((void *)(gCap1EcapBase + CSL_ECAP_CAP1));
    //    edmaParam2.destAddr      = (uint32_t) SOC_virtToPhy((void *) capTrigTimeStamps);
    //    edmaParam2.aCnt          = (uint16_t) (APP_EDMA_A_COUNT);
    //    edmaParam2.bCnt          = (uint16_t) (APP_NUM_CAP_TRIG_REG_TRANSFER);
    //    edmaParam2.cCnt          = (uint16_t) (APP_NUM_CAP_TRIG_TRANSFERS);
    //    edmaParam2.bCntReload    = 0;
    //    edmaParam2.srcBIdx       = (int16_t) EDMA_PARAM_BIDX(APP_EDMA_A_COUNT);
    //    edmaParam2.destBIdx      = (int16_t) EDMA_PARAM_BIDX(APP_EDMA_A_COUNT);
    //    edmaParam2.srcCIdx       = (int16_t) 0;
    //    edmaParam2.destCIdx      = (int16_t) APP_EDMA_A_COUNT * APP_NUM_CAP_TRIG_REG_TRANSFER;
    //    edmaParam2.linkAddr      = 0xFFFFU;
    //    edmaParam2.srcBIdxExt    = (int8_t) EDMA_PARAM_BIDX_EXT(0);
    //    edmaParam2.destBIdxExt   = (int8_t) EDMA_PARAM_BIDX_EXT(0);
    //    edmaParam2.opt           = (EDMA_OPT_TCINTEN_MASK | EDMA_OPT_SYNCDIM_MASK |
    //                              ((((uint32_t)(gEdmaTcc[1])) << EDMA_OPT_TCC_SHIFT) & EDMA_OPT_TCC_MASK));
    //
    //    EDMA_setPaRAM(gEdmaBase, param1, &edmaParam2);
    
    
    //    EDMA_linkChannel(gEdmaBase, gEdmaPaRams[0], param0);
    //    EDMA_linkChannel(gEdmaBase, gEdmaPaRams[1], param1);
    
    
    
        EDMA_linkChannel(gEdmaBase, gEdmaPaRams[0], gEdmaPaRams[0]);
        EDMA_linkChannel(gEdmaBase, gEdmaPaRams[1], gEdmaPaRams[1]);
    
    
        for(int iter = 0; iter < APP_NUM_EDMA_CHANNELS; iter++)
        {
            EDMA_configureChannelRegion(gEdmaBase, gEdmaRegId, EDMA_CHANNEL_TYPE_DMA,
                gEdmaChannels[iter], gEdmaTcc[iter], gEdmaPaRams[iter], EDMA_TEST_EVT_QUEUE_NO_0);
        }
    
    }
    
    void App_edmaDeConfig(void)
    {
        int32_t status = SystemP_SUCCESS;
    
        for(int iter = 0; iter < APP_NUM_EDMA_CHANNELS; iter++)
        {
            EDMA_freeChannelRegion(gEdmaBase, gEdmaRegId, EDMA_CHANNEL_TYPE_DMA,
                gEdmaChannels[iter], gEdmaTcc[iter], gEdmaPaRams[iter], EDMA_TEST_EVT_QUEUE_NO_0);
    
            status = EDMA_freeDmaChannel(gEdmaHandle[0], &(gEdmaChannels[iter]));
            DebugP_assert(status == SystemP_SUCCESS);
            status = EDMA_freeTcc(gEdmaHandle[0], &(gEdmaTcc[iter]));
            DebugP_assert(status == SystemP_SUCCESS);
            status = EDMA_freeParam(gEdmaHandle[0], &gEdmaPaRams[iter]);
            DebugP_assert(status == SystemP_SUCCESS);
        }
    }
    
    bool App_compareInRange(uint32_t input1, uint32_t input2, uint32_t error_range)
    {
        uint32_t absDiff = (input1 > input2)? (input1 - input2): (input2 - input1);
        if(absDiff <= error_range)
        {
            return true;
        }
        return false;
    }
    
    

  • Hi Sue,

    Please refer to this Academy lab on DMA configuration for continuous mode:

    dev.ti.com/.../node