This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4-Q1: failed MCAN communication using SDK example(mcan_external_read_write)

Part Number: AM263P4-Q1
Other Parts Discussed in Thread: SYSCONFIG, TMDSCNCD263P

Tool/software:

Dear Champs,

My customer is trying to test MCAN using SDK example(mcan_external_read_write) on AM263Px control EVM(CCEVM), and found there was stuck occurred in below 'SemaPhoreP_pend()' function.

When they checked RAM, there is no data in RX buffer, but there is data in TX buffer.

When they checked J5 pin1 and pin3 of CC EVM for MCAN4, there is no signal was observed,

There are no signal observed as below.

Their SW is mcu_plus_sdk_am263px_10_01_00_31, and they build and exceute this example using CCS20.1.1.

Their Sysconfig setting is as below.

Thanks and Best Regards,

SI.