Part Number: MSPM0G3507-Q1
Other Parts Discussed in Thread: BQ76907-Q1, MSPM0-SDK
Tool/software:
Hello Expert
We have BMS requirement of sleep mode current limit < 50 µA for entire battery pack.
I was checking bq769x0 Boot Switch Alternatives out of which microcontroller controlled (Figure 1. Independently Powered MCU Boot) looks promising as of now at high level.
Idea is to shutdown AFE and keep MCU in standby mode to lower current consumption.
To wakeup I am thinking two ways
- Wakeup via CAN: Use CAN wakeup pattern by connecting MCU GPIO and CAN RXD to wakeup MCU from Standby to RUN mode
- Wakeup by load connect: Use MCU COMP0/1/2 across PACK- and GND (may be like AFE CHG detector logic BQ76907-Q1) to detect load connect on PACK+ and PACK-
Please let me know any application note on similar design requirement as well as your thoughts.
Best Regards,
Tirthraj