Part Number: MCU-PLUS-SDK-AM263PX
Tool/software:
Hi,
I’m working with the AM263Px CC evaluation board and the AM263x controlCARD Dock. I tried to run the ADC example ‘ADC SOC Continuous’ from the SDK version mcu_plus_sdk_am263px_10_00_00_35. I feed the ADC 1 Channel 0 (HSEC_ADC1_AIN0) with the variable resistor output ADC_POT2_OUT. When I run the executable in CCS (version 12.8.1), I get the following error:
[Cortex_R5_0] ASSERT: 0.863s: syscfg/ti_drivers_config.c:System_init:224: SOC_getAdcReferenceStatus(1) == true failed !!!
Where does the error come from? What does it mean and how can I fix it?
Regards,
Wega