Part Number: TMS570LC4357-EP
Tool/software:
Hi,
In figure 12.27 of TMS570LC4357-EP Reference Manual, the EMIF connection with external Flash memory has been shown.
There are two things what we observed (may be connection mistakes) in this connection -
1) The data bus is connected in straight fashion without byte swapping as mentioned in TMS570LC4357-EP Datasheet section 5.14 NOTE.
2) In an address bus connection, Address line ADD]12] is missing form microcontroller side.
Is this ( figure 12.27) connection of external flash memory is correct?
If not, I feel TRM is not written properly and should be corrected.
Regards,