This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: Doubts in mcrc code

Part Number: AM2634

Tool/software:

Hi jagadish,

I updated the CRC type to SAE J1850, changed the data bit size from 64-bit to 8-bit, set params.dataBitSize to 1, and changed the gMCRC data buffer size from 400 to 1, assigning the value 35 directly as shown below. I used a debug log print statement to read the SectSign register values, as shown below.

After performing a hardware reset, I dumped this code and got a result of 160 the first time. Then I clicked on reset option and then start icon in order to run code again from the start ; this time, I got a new result of 225.
Tell me where I am going wrong. Do I need to include any API at the start of the code to reset the MCRC module? Because only after doing a hardware reset am I getting the expected value