Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
My customer has problems on IPC communication. Could you please help them to solve the following issues ?
In the System Configuration Tool, when the communication between CPU cores is set to "IPCNotify + IPC RP Message", the "IPC_shared_MEM_size" in the automatically generated source code is set as “0”.
In addition, the definition of the IPC memory area is "gIpcSharedMem[]" in the initialization process, then the compile error occurred.
How can they set IPC_shared_MEM_size which they want in the System Configuration Tool ?
Can they also configure which area of gIpcSharedMem[] is used for each CPU core?
They’re using the following tools.
・SysConfig: 1.23.1+4034
・Code Composer Studio:12.8.1.00005
・SDK:motor_control_sdk_am243x_09_02_00_11
Thanks and regards,
Hideaki