This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4-Q1: AM263P4-Q1

Part Number: AM263P4-Q1

Tool/software:

I am trying to verify the R5F core clock configuration on the AM263Px using GEL scripts. My objective is to switch between 400 MHz and 200 MHz clock configurations and verify them using the CycleCounterP_getCount32() API inside periodic RTI ISRs.

I used GEL scripts to configure the R5 clock:

  • For 400 MHz configuration, the register CFG0_R5SS0_CLK_DIV_SEL is set to 0x0.

  • For 200 MHz configuration, the same register is set to 0x1.

I confirmed these settings by reading the CFG0_R5SS0_CLK_DIV_SEL register after applying the GEL scripts.

I used the CycleCounterP_getCount32()  API  inside the RTI interrupt service routines to measure cycle counts under both configurations.

Test Case RTI Period Clock Config API Used
TC_01 1 ms 400 MHz CycleCounterP_getCount32()
TC_02 1 sec 400 MHz CycleCounterP_getCount32()
TC_03 1 ms 200 MHz CycleCounterP_getCount32()
TC_04 1 sec 200 MHz CycleCounterP_getCount32()

Despite changing the clock divider (0x0 vs. 0x1), the cycle count observed in both configurations remains the same.Attached the observations.