This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] MSP Hardware Development Resources

[Click here to return to homepage]

MSPM0 HARDWARE DEVELOPMENT

Listed below are a variety of documents and FAQs to assist with the physical implementation of MSPM0 devices


Layout and Design Tips

(Hardware development guidance, passive layout, )

Documentation FAQs
  • FAQs here

Noise/EMC Resources

(Reducing noise/EMC, proper testing procedures, cleaning ADC signals)

Documentation FAQs
  • FAQs here

Power Optimization

(Low power optimization, power domains)

Documentation FAQs
  • FAQs here

Reference Designs

Links
  • TIDA-010279 - 1500V Stackable battery management unit
  • TIDA-010940 - Single-phase e-meter with LCD and magnetic tamper detection
  • TIDA-010264 - Medical alarm with supercapacitor backup
  • TIDA-010941 - Smoke detector with ambient light rejection
  • TIDA-010250 - 1kW BLDC motor inverter (sensored or sensoreless motor control)