Part Number: SYSCONFIG
Tool/software:
Dear TI team,
when trying to configure the OSPI flash driver for a custom flash I attempted to use the "LOAD FROM JSON" feature to import a JSON file generated with ospi_flash_diag, but using MCU+ SDK 11.0 / SysConfig 1.22.0 I'm getting an error ("ReferenceError: eclipseOpenBrowseFileDialog2 is not defined"):

Using the same CCS installation (12.8.1) and MCU+ SDK 10.01 / SysConfig 1.21.2, it works:

Since MCU+ SDK 10.01 with SysConfig 1.22.0 fails the same as MCU+ SDK 11.0, I'm guessing the culprit is in SysConfig 1.22.0.
Is this a known issue?
Are there any known workarounds?
Regards,
Dominic