Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4-Q1: AM263P4-Q1

Part Number: AM263P4-Q1
Other Parts Discussed in Thread: AM263P4, SYSCONFIG

Tool/software:

I am trying to use UART5 of AM263P4 launchpad and configured it using System Configuration to use the pins J1.3 and J1.4 which are UART5 Tx and Rx pins. After configuring ,on checking the voltage levels at U54 UART/EPWM mux sel pin (1) It is high (3.2v) and UART/EPWM MUX EN pin is low , which means EPWM is getting configured even though i am trying to configure it as UART5 Tx and Rx pins. 

How to resolve this?