Part Number: MSPM0G3107-Q1
Tool/software:
Hi,
Greetings!
We are new to working with the MSPM0G3107-Q1 microcontroller.
We would like to know if we can use a 20 MHz crystal with the MSPM0G3107-Q1 (Package: LQFP-64) on the HFXT input.
Proposed Crystal Part Numbers:
-
CTS Corporation – 403C11A20M
-
TXC Corporation – 7M20 000MEEQ
(Specs: 20.000 MHz, 10 pF load capacitance, ±30 ppm, 3.2 × 2.5 mm, RoHS compliant)
Additionally, we would like to confirm:
-
Is it mandatory to use an external LFXT for low-frequency applications, or can the internal oscillator suffice?
Looking forward to your guidance.
Best regards,
Aditya